This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: LAUNCHXL-CC26X2R1 No one of the nodes identified as RTLS MASTER

Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: CC2642R

Dear Expert ,

Good day!

Our customer use the LAUNCHXL-CC26X2R1 to test the AOA , But they meet an error “No one of the nodes identified as RTLS MASTER” , after their software engineer debug , it shown "1 nodes not identified at all" . the details please refer to the picture below :

The test setting is shown below :

Python 3.7.4

SDK: simplelink_cc13x2_26x2_sdk_3_40_00_02

LAUNCHXL-CC26X2R1 +BOOSTXL-AOA

I had check the similar query 

e2e.ti.com/.../launchxl-cc26x2r1-rtls_example_with_rtls_util-py-raise-error-error-no-one-of-the-nodes-identified-as-rtls-master

Except this , could you provide more suggestions?

BR,

Leon.liu

  • Hi Expert ,

    One more query , how to enter the  iBeacon Receiving and transmitting modes.

    Do you have the source bin file ?

    BR.

    Leon.liu

  • Hi Leon,

    Is there a reason why they are using such an old SDK. I would recommend to evaluate the project using SDK 5.10 or 5.20.

    When it comes to the AoA example, have they followed the guidance on the proper SimpleLink Academy labs and/or in the README file provided within the RTLS_Agent?

    I am referring to the COM port used. This one should be changed within the python script accordingly with the COM port allocated by the computer to the CC2642R board.

    Best regards,

  • Hi Expert ,

    One more query , how to enter the  iBeacon Receiving and transmitting modes.

    Do you have the source bin file ?

    BR.

    This question is not related to this thread. Please open a separate thread. This helps having the proper experts affected to your query and ease the search process for other users. Thank you for your comprehension,

    Best regards,