This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: External Antenna for CC2652

Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: CC1352R, CC2652R

Hi

I am having difficulty finding an external 2.4GHZ antenna that mounts onto the MM5829-2700 connector on the LAUNCHXL-CC26X2R1 board. Do you have any recommended antennas with mating connector?

Best,

Martin

  • Hi Martin,

    I usually use this kind of connector when I want to use an external antenna with the LAUNCHXL-CC26X2R1 board. After this, I use an SMA antenna.

    The second option could be to go for a LAUNCHXL-CC1352R1 as this launchpad has a SMA antenna port. (Note: all the code interfacing the 2.4 GHZ stacks written for CC2652R should be compatible with CC1352R devices, the caveat might be in the pin mapping used).

    I hope these will help,

    Best regards,