Other Parts Discussed in Thread: UNIFLASH, CC2652R
I have an application on this processor where the client wishes to update the application firmware while
leaving the RTOS and BLE firmware versions unchanged. Is there an method to OAD just the application
firmware or is it only possible to do the entire binary image including the RTOS/BLE components?
A side question, I am using Launchpad CC26x2R1. On my actual product board which is running now
and the BLE works to connect to a smart phone. On my board I did not include the extra memory part
which is connected to the CPU via. SPI and appears to be a location where a 'factory image' is stored
and maybe reloaded based on the buttons at boot time. Use of this external memory part for image
loading or re flashing, is it needed for OAD as I wish to do? I hope not as the SPI pins are used
for I2S in my application as well as no other pins available to move SPI to for that memory use.
Any links to additional documentation to do what I need and/or video training would be great!
TI's web site is huge and I've been stumbling around reading to get up on this issue, some of the
docs are old and you don't find that out until reading almost the whole thing, I wish to use the latest
SDK and RTOS components as well as your latest libraries to build this product. I think I remember
having seen some app. note or other PDF which talked about loading just application firmware vs.
the entire image. Today now that my board is running and I need to finish this function I can't find
the reference that led me to select the TI part and RTOS over a year ago.
Thanks in advance, Marc Y./MySoftworks Co.