This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Bluetooth Mesh questions

Genius 5895 points
Part Number: CC2642R

Hi,

I'm learning Bluetooth Mesh and see this article.
www.ti.com/.../swat016a.pdf

Question 1:
The range of Bluetooth Mesh is Up to 200m.
Does this mean that the distance between each node is 200m?
Which is correct, ① or ②?

Question 2:
Can we use Bluetooth Mesh in Long Range mode?
Generally, the maximum communication range of BLE is 200m, and LR mode is 400m. In this article of Bluetooth Mesh, it is written 200m.

Is it possible for TI devices to communicate bluetooth mesh in the 400m range(LR mode)?

Best regards,

Rei