Issues:
1. No connected AOA: IQ escalation is via the event RTLSSRV_CL_CTE_IQ_REPORT_EVT. The customer has checked the code of this section, and do not find a data structure which can distinguish the mac address, and this will result in an IQ data on which device is unknown.
For one master and multiple slaves synchronized, is there only one or more syncHandles?
If the customer would like to determine different mac devices, what fields should the customer use?
2. Based on the example of cc26x2 5.1sdk, the customer would like to know the source code file for calculating the angle for reference.
Thanks!
Best Regards,
Cherry Zhou