Dear Team,
We are planning to used CC2642R BLE controller for our new project. As per project requirement we are planning to use color sensor AS7261 which is interface with the CC2642R controller either on UART or I2C interface.
The calibrated white data from color sensor in the form of • XYZ, • xy data (CIE 1931), • DUV, u’v’, uv (CIE 1976), • CCT, LUX.
Below are the queries
1. The concern is that can we convert above raw data file in RGB data format? CC2642R is capable to run that algorithm?
2. Can we connect 16MB or 64MB SPI NOR flash with this CC2642R BLE controller, Memory mapping can be possible by this BLE controller.?
Waiting for your response.