Other Parts Discussed in Thread: RF430FRL152H
Hello,
I had now initiated without errors, and successfully scanned in BTool after Host_Test device flashing/unplugging/plugging. But the list of Slave BDA (2C:00:16:2B:00:5A, for example) does not seem to match the device (GAP) address (0C:61:CF:47:63:53), obtained from PuTTy terminal (COM4) while flash the device with Project Zero. Besides, selecting/filling either of the addresses in Salve BDA area did not seem to establish connection successfully, with following messages:
[when selecting 2C:00:16:2B:00:5A from the dropdown]: Please note that status is "bleincorrectmode."
[21] : <Rx> - 12:51:00.654
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x14 (20) bytes(s)
Event : 0x0605 (1541) (GAP_EstablishLink)
Status : 0x12 (18) (bleIncorrectMode)
DevAddrType : 0x02 (2) (ADDRTYPE_PUBLIC_ID)
DevAddr : 2C:00:16:2B:00:5A
ConnHandle : 0x0000 (0)
ConnRole : 0x00 (0) (
ProfileRoles Bit Mask Is Not Set)
ConnInterval : 0x0000 (0)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0000 (0)
ClockAccuracy : 0x00 (0)
Please note that status is "bleincorrectmode." Does this mean BLE is in correct mode or incorrect mode?
[when filling the device address 0C:61:CF:47:63:53 in the Slave BDA area]:
[26] : <Rx> - 12:54:02.938
-Type : 0x04 (Event)
-EventCode : 0x00FF (HCI_LE_ExtEvent)
-Data Length : 0x14 (20) bytes(s)
Event : 0x0605 (1541) (GAP_EstablishLink)
Status : 0x09 (9) (NV_ITEM_UNINIT)
DevAddrType : 0x02 (2) (ADDRTYPE_PUBLIC_ID)
DevAddr : 0C:61:CF:47:63:53
ConnHandle : 0x0000 (0)
ConnRole : 0x00 (0) (
ProfileRoles Bit Mask Is Not Set)
ConnInterval : 0x0000 (0)
ConnLatency : 0x0000 (0)
ConnTimeout : 0x0000 (0)
ClockAccuracy : 0x00 (0)
Please note the status is "NV_ITEM_UNINIT". It mean it's un-initiated, right??
Furthermore, the COM4 port in the PuTTy terminal turned "inactive" or "unable to connect", after BTool is activated for scanning or connection establishing. So it would not show any "connected" PuTTy status as depicted in training step 2 (Using BTool).
What could be the problems? Thank you very much!
Albert