This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-CC26X2R1: BTOOL testing issue in DTM mode.

Part Number: LAUNCHXL-CC26X2R1
Other Parts Discussed in Thread: CC2652RB

Hi,

I am trying to connect CC26X2R1 LP with CC2652RB LP using BTOOL. I have used host_test (DTM mode)project from simplelink_cc13x2_26x2_sdk_4_10_00_78 and flashed on CC26X2R1 LP. Similarly on CC2652RB i have flashed simple_periheral example project.

When i connect BTOOL to CC26X2R1 LP i see "Device Reset Timeout" error.

Later when i click on Scan button in BTOOL the CC2652RB device is not visible in the scanned device list. I am able to see CC2652RB beacons on BLE scanner app.

Need help in debugging this issue.

Regards

Pratik

  • Hi Pratik,

    It looks like the commands sent to the CC26x2R device are not properly received. Here is a list of the elements you may want to verify:

    • Once the device has been flashed, make sure to unplug the device and re-plug it.
    • Please verify you are using the proper COM port to interface the device and that is properly set. Below are the settings I am using.
    • Check if all the jumpers - especially the jumpers named "Rx" and "Tx" - are properly set.
    • Try to reset the device using the reset button on the launchpad

    I hope this will help,

    Best regards,