Hello,
İs Three a simple project which is send uart receiving data on ble and send ble receiving data to uart ?
İs there any document tutorial for ble programing.
Best regards..
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
İs Three a simple project which is send uart receiving data on ble and send ble receiving data to uart ?
İs there any document tutorial for ble programing.
Best regards..
Hello OOMAR,
You can evaluate the Host Controller Interface, starting with the host_test project. I also recommend that you complete each Bluetooth 5 SimpleLink Academy Lab.
Regards,
Ryan
Hello Ryan
Host_test project is have some compile error and file error.
May you send me full project(host_test) or any other prohects
Best regards
I did not encounter any similar issues when building the out-of-box host_test project, please make sure you are using the correct SDK dependencies as stated in the Release Notes. You may consider completing a re-install to determine whether this can resolve the issue.
Regards,
Ryan
Hello Ryan,
Other forum post solve my problem, Fistly I build "Stack_Wrapper" than I build "host_test".
But I did not understand sending data on uart yet.
May you prefer me some more tutorial or examples projects?
Best Regards.
You can review the NPI/Transport folder to further understand the npi_tl layer, configuration, and UART module. More information is provided in the BLE5-Stack User's Guide in regards to NPI functionality. If planning to use a single-chip solution, you could remove the DISPLAY feature from another example such as simple_peripheral and add your own UART bi-directional layer using the UART TI Driver API.
Regards,
Ryan