I Am using CC2652RB Launch board and In CCS I am getting issues regarding Building the own program, when I am using Examples they are working properly. But for my own code .OUT files are not generating.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I Am using CC2652RB Launch board and In CCS I am getting issues regarding Building the own program, when I am using Examples they are working properly. But for my own code .OUT files are not generating.
Hi D Manikanta,
What example are you building your program from? I would suggest importing an existing LP-CC2652RB project to work from. Output settings should be defined by Project Properties -> Build -> Arm Linker.
Regards,
Ryan
I am Imported Project Zero Example, Example programs are executing. But, if i create new project in CCS tool then while Building the program .OUT file not generating after Output Settings changed as you said.
I Also re installed the CCS tool for 2 times, Same output.Not only in Company PC also in Mypersonal laptop same NO output.
It is always recommended that developers start by importing a SimpleLink SDK example to start your project from, like the empty TI Driver example. If Project Properties -> Build -> Arm Linker -> Basic Options -> Specify output file name does not contain a location (like ${ProjName}.out) then the output file will not be generated.
Regards,
Ryan
Please clean/rebuild the project and check your output folder, the same location where the .map file should be generated.
Regards,
Ryan
Is their any choice of missing libraries can be download or else we need to reinstall the entire CCS tool again a sir.
As you said sir .map file is generated but still some errors.
In the beside image as you said sir .map file is generated but also .out file error can be seen.
The output file will not be generated since the link step fails and thus the build does not complete. The correct libraries will be included when you import an existing example project, which you can then modify to fit your application needs. It is not recommended to create a new project from scratch and you are not required to reinstall CCS.
Regards,
Ryan
For some extent its ok, what if I need to add more different files for my project.
It is not recommended to create a new project from scratch.
But for a fresher need to write new program for gpio pins for blink led, then how???