Other Parts Discussed in Thread: CC2652RB
Hi TI,
I use simplelink_cc13x2_26x2_sdk_4_30_00_54\examples\rtos\CC2652RB_LAUNCHXL\drivers\empty with LP_CC2652RB.
The example is working well, however when I add a NVS module, it can't work.
The module config as below:
After add the module, build and flash, the content of flash as following:
The yellow bytes mean the backdoor mode is enable and the start address is NOT correct.
If I change above 5 bytes to 0 and write it, the firmware is working well again.
I want know why and how to disable the backdoor mode.
This is very urgent and important for our project, thanks very much!