Hi Team,
Here's an issue from the customer may need your help:
The customer would like to use the cc2640r2f for data transfer of the bmd101 heart. The bmd101 sends a packet every 2 ms, 8 bytes each. To transfer data to a mobile phone using cc2640r2f via notify, and to achieve a transmission rate of 5 kb/s, the test bmd101 data was too large to allow the cc2640r2f to transfer data to the mobile phone.
Is there any routine that directly enables high-speed data transmission?
Could you help check this case? Thanks.
Best Regards,
Cherry