Other Parts Discussed in Thread: CC2652RSIP, SYSCONFIG
I have been having problems with SimpleLink SDK 5.40.00.40 and greater.
One issue I have seen is changing the Address Mode from RPA with Public ID to Random Static Address using SysConfig works fine using the example simple_peripheral_LP_CC2652RSIP_tirtos_ccs from the 5.30.01.01 SDK, but breaks the BLE in example simple_peripheral_LP_CC2652RSIP_tirtos7_ticlang from the 6.10.0.29 SDK. If you change the Address Mode from RPA with Public ID to Random Static Address in the 6.10 SDK you don't see advertisements over the air.
Another issue with SDK 5.40 and greater, which I haven't been able to reproduce using one of the example projects, is the ICall task blocks when you try to make a connection and never unblocks and subsequently the BLE connection is broken and advertising is also broken. I have found a workaround, which is replacing the ti_radio_config.c file generated by SysConfig with a ti_radio_config.c generated using the 5.30.01.01 SDK. I don't know if these issues are related.
Best regards,
Steve