Other Parts Discussed in Thread: CC1352P, SYSCONFIG
Hi,
Our Transmitter(CC2652P) are transmitting at 100 data packets per second to RX (CC1352P4). From 4 Tx i.e. 400 data packets per seconds.
As per my previous thread I got to know that SDK 4.2 doesn't support high PA which was a Bug. I upgraded my SDK to 5.1 and saw a good RSSI and checked the same on RF Analyzer and it was active.
But,
This change in SDK has lead to dropping of data that I received in CC1352P from 4 slaves (CC2652P). With Earlier SDK I was able to get 98% data on Bench test and 90% in Automotive Environment. But with new SDK I was able to see MAX- 70% data. I saw the slaves are connected but unable to send data.
1. Why is this issue with new SDK. Which I saw is that the Slaves are Unable to send data for 20- 50 seconds which is very critical. As per the Migration Guide I have copied all Application files Including Simple Peripheral.c and .h and just copied sysconfig manually.
2. My SDK on Tx is 5.1 and Rx is 4.2 will this effect in frequency.
3. In SDK 5.1 I have seen an option to disable Update Parameters. But once I disable the Update parameter on Tx side I see this error.
Please suggest solutions to this.
Regards