Other Parts Discussed in Thread: SYSCONFIG
Hi team,
SDK:simplelink_cc13xx_cc26xx_sdk_6_10_00_29.
examples:simple_central and simple_peripheral
The Customer used two LAUNCHXL-CC26X2R1 boards to test Connectable directed advertising.
He found no advertisement and wasn't able to connect to Central successfully. I can reproduce this.
the following is sysconfig settings:
advParams1:
Legacy Event Properties Option: Connectable directed
Peer Address Type: Public Or Public ID
Peer Address: 80:6F:B0:2B:33:10 (This is the Dev Addr of simple_central: 0x806FB02B3310)
Filter Policy: Process requests from all devices
Both the Central and Peripheral are set to Public Address.
Could you help to check this?
Regards,
Kevin