hi:
when i use simple central example to do some scan test, here is something bad happened.
device:LP-CC1352P7: sdk:6.10
1. first, change the scan parameter with GapScan_enable(0x0, 0, 0x20); rebuild the project, and load it to the launchpad. press the button of lanchpad to trigger scan, it works,,but it only repoort serveral device even i am waiting for five minutes.
2. second, press the button to terminate scan, it works
3. third, press the button to re-scan, it doesn't work, and it has no responce to any operation of buttton, it seems the ble stack doesn't work and it can recover only in reboot operation
according to the phenomenon discribed above, the scan peration seems not stable. can you help me to fix this issue.
thanks!