We have the EXP430F5438 with the PAN1315ETU and with the accl.d43 application loaded as supplied in the SDK. It has been demonstrated to pair with another identical board.
We have assumed it can pair with a PC. There is a bluetooth Cirago USB dongle on the PC which appears to use a Toshibia stack. In the "Add New Connection Wizard" it finds the device "BlueMSP-DemoDCC2". then when one selects that device for connection the message "Detection of service failed" appears with no indication of what service failed.
It appeared that the demo program and stack at least supported the SPP profile which should be sufficient.
Should the demo program pair with a PC? if not, what needs to be done to the demo program so it will if that is possible?