Part Number: CC2642R
Hi,
I created a project in SCS to use the COMPA and COMPA event trigger. To do that a linked the COMPA to the DIO30. DIO30 is an ADC powered with 3.3V. My trigger is set to occurs when the DIO30 falling edge. Everything works fine in SCS. I can see the event and the compaValue that changes.

But when I created a project in CCS (To do this I used the empty project in the skd drivers folder) and included the scif framework generate by the SCS, the compaValue starts with 0 (it should starts with 1 as we can see in the SCS) and I can't see the event happen.
When I look the DIO30 input, the value read is 0:

This is my code for the version sdk 3.40:
#include "ex_include_tirtos.h"
#include "scif.h"
#define BV(n) (1 << (n))
// Display error message if the SCIF driver has been generated with incorrect operating system setting
#if !(defined(SCIF_OSAL_TIRTOS_H) || defined(SCIF_OSAL_TIDPL_H))
#error "SCIF driver has incorrect operating system configuration for this example. Please change to 'TI-RTOS' or 'TI Driver Porting Layer' in the Sensor Controller Studio project panel and re-generate the driver."
#endif
// Display error message if the SCIF driver has been generated with incorrect target chip package
#ifndef SCIF_TARGET_CHIP_PACKAGE_QFN48_7X7_RGZ
#error "SCIF driver has incorrect target chip package configuration for this example. Please change to 'QFN48 7x7 RGZ' in the Sensor Controller Studio project panel and re-generate the driver."
#endif
// Task data
Task_Struct myTask;
Char myTaskStack[1024];
// Semaphore used to wait for Sensor Controller task ALERT event
static Semaphore_Struct semScTaskAlert;
volatile uint16_t before_state;
volatile uint16_t after_state;
/*OPEN_CNT | PIN_INPUT_EN | PIN_PULLDOWN | PIN_HYSTERESIS,CLOSE_CNT | PIN_INPUT_EN | PIN_PULLDOWN | PIN_HYSTERESIS,*/
const PIN_Config pwr_fail_PinTable[] = {
IOID_20 | PIN_INPUT_EN | PIN_GPIO_LOW | PIN_DRVSTR_MAX,
PIN_TERMINATE
};
PIN_State pwr_fail_PinState;
void scCtrlReadyCallback(void) {
} // scCtrlReadyCallback
void scTaskAlertCallback(void) {
// Wake up the OS task
Semaphore_post(Semaphore_handle(&semScTaskAlert));
} // scTaskAlertCallback
void taskFxn(UArg a0, UArg a1) {
PIN_Handle pwr_fail_PinHandle;
pwr_fail_PinHandle = PIN_open(&pwr_fail_PinState, pwr_fail_PinTable);
// Initialize the Sensor Controller
scifOsalInit();
scifOsalRegisterCtrlReadyCallback(scCtrlReadyCallback);
scifOsalRegisterTaskAlertCallback(scTaskAlertCallback);
scifInit(&scifDriverSetup);
before_state = scifTaskData.compaTask.output.compaValue;
scifStartTasksNbl(BV(SCIF_COMPA_TASK_TASK_ID));
// Main loop
while (1) {
PIN_setOutputValue(pwr_fail_PinHandle, IOID_20, 0);
// Wait for an ALERT callback
Semaphore_pend(Semaphore_handle(&semScTaskAlert), BIOS_WAIT_FOREVER);
// Clear the ALERT interrupt source
scifClearAlertIntSource();
PIN_setOutputValue(pwr_fail_PinHandle, IOID_20, 1);
after_state = scifTaskData.compaTask.output.compaValue;
// Acknowledge the alert event
scifAckAlertEvents();
}
} // taskFxn
int main(void) {
Task_Params taskParams;
// Initialize the board
Board_initGeneral();
#ifdef Board_shutDownExtFlash
Board_shutDownExtFlash();
#endif
// Configure the OS task
Task_Params_init(&taskParams);
taskParams.stack = myTaskStack;
taskParams.stackSize = sizeof(myTaskStack);
taskParams.priority = 3;
Task_construct(&myTask, taskFxn, &taskParams, NULL);
// Create the semaphore used to wait for Sensor Controller ALERT events
Semaphore_Params semParams;
Semaphore_Params_init(&semParams);
semParams.mode = Semaphore_Mode_BINARY;
Semaphore_construct(&semScTaskAlert, 0, &semParams);
// Start TI-RTOS
BIOS_start();
return 0;
} // main
And for the sdk 6.10:
#include "ex_include_tirtos.h"
#include "scif.h"
#define BV(n) (1 << (n))
// Display error message if the SCIF driver has been generated with incorrect operating system setting
#if !(defined(SCIF_OSAL_TIRTOS_H) || defined(SCIF_OSAL_TIDPL_H))
#error "SCIF driver has incorrect operating system configuration for this example. Please change to 'TI-RTOS' or 'TI Driver Porting Layer' in the Sensor Controller Studio project panel and re-generate the driver."
#endif
// Display error message if the SCIF driver has been generated with incorrect target chip package
#ifndef SCIF_TARGET_CHIP_PACKAGE_QFN48_7X7_RGZ
#error "SCIF driver has incorrect target chip package configuration for this example. Please change to 'QFN48 7x7 RGZ' in the Sensor Controller Studio project panel and re-generate the driver."
#endif
// Task data
Task_Struct myTask;
Char myTaskStack[1024];
// Semaphore used to wait for Sensor Controller task ALERT event
static Semaphore_Struct semScTaskAlert;
volatile uint16_t before_state;
volatile uint16_t after_state;
void scCtrlReadyCallback(void) {
} // scCtrlReadyCallback
void scTaskAlertCallback(void) {
// Wake up the OS task
Semaphore_post(Semaphore_handle(&semScTaskAlert));
} // scTaskAlertCallback
void taskFxn(UArg a0, UArg a1) {
//Power fail: config DIO20 as output
GPIO_setConfig(CONFIG_GPIO_20, GPIO_CFG_OUT_STD | GPIO_CFG_OUT_LOW);
// Initialize the Sensor Controller
scifOsalInit();
scifOsalRegisterCtrlReadyCallback(scCtrlReadyCallback);
scifOsalRegisterTaskAlertCallback(scTaskAlertCallback);
scifInit(&scifDriverSetup);
before_state = scifTaskData.compaTask.output.compaValue;
scifStartTasksNbl(BV(SCIF_COMPA_TASK_TASK_ID));
// Main loop
while (1) {
//Power fail: clean DIO20
GPIO_write(CONFIG_GPIO_20, 0);
// Wait for an ALERT callback
Semaphore_pend(Semaphore_handle(&semScTaskAlert), BIOS_WAIT_FOREVER);
// Clear the ALERT interrupt source
scifClearAlertIntSource();
//Power fail: set DIO20
GPIO_write(CONFIG_GPIO_20, 1);
after_state = scifTaskData.compaTask.output.compaValue;
// Acknowledge the alert event
scifAckAlertEvents();
}
} // taskFxn
int main(void) {
Task_Params taskParams;
// Initialize the board
Board_initGeneral();
#ifdef Board_shutDownExtFlash
Board_shutDownExtFlash();
#endif
// Configure the OS task
Task_Params_init(&taskParams);
taskParams.stack = myTaskStack;
taskParams.stackSize = sizeof(myTaskStack);
taskParams.priority = 3;
Task_construct(&myTask, taskFxn, &taskParams, NULL);
// Create the semaphore used to wait for Sensor Controller ALERT events
Semaphore_Params semParams;
Semaphore_Params_init(&semParams);
semParams.mode = Semaphore_Mode_BINARY;
Semaphore_construct(&semScTaskAlert, 0, &semParams);
// Start TI-RTOS
BIOS_start();
return 0;
} // main
I tried to generate the code with the Sensor Controller Studio: Version 2.6.0.132 (simplelink_cc13x2_26x2_sdk_3_40_00_02) and 2.9.0.208 (simplelink_cc13xx_cc26xx_sdk_6_10_00_29).
Code Composer Studio Version is 11.1.0.00011.
Thanks in advance,
Cristiane Bellenzier Piaia