Hi team,
Here's an issue from the customer may need your help:
In lab tests of board frequency deviation, a 50-Hz line frequency disturbance was found in the 32.768-kHz crystal, as shown in the following figure:
PCB layout is as the following figure:
1) Is the case because the RF link and crystal are too close together? Is there any other way to solve this problem than increasing the distance between the two? How much does the issue affect Bluetooth communication?
2) CC2652RB has Baw inside, but in Bluetooth configuration, it's not able to divide by Baw, only RCOSC_LF is the clock source. Is it possible to switch to Baw divide?
Thanks.
Best Regards,
Cherry