Hi,
I have a question about OAD speed.
My customer is using the on-chip OAD and SDK version is v4.40.04.04.
The image size is about 200KB, and the download time is about 3 to 4 minutes.
He wants to reduce time.
We set the OAD block size to maximum to reduce time.
And the PDU size is also set to the maximum, and the connection interval is 800.
But there was no change in speed and time.
How can I speed up OAD?