Other Parts Discussed in Thread: CC2642R, LAUNCHXL-CC26X2R1
Hello,
I encountered a lot of problems using EnergyTrace in CCS (11.2.0.00007) with a XDS110 debugging a CC2642R.
1) When using "probe supplied power", I start a debug session, then open EnergyTrace, then run the code.
EnergyTrace gets stuck on the first value of the timer and no value changes nor trace appear on the graphs.
Target configuration used :
EnergyTrace :
2) When using "Target supplied power", I start a debug session, then open EnergyTrace, then run the code.
The "EnergyTrace Technology" tab displays "Stream closed"
Target configuration :
EnergyTrace :
3) When stopping a debug session, the "EnergyTrace Technology" tab closes, and the "Energy" and "Current" graph tabs stay.
4) I often get the "Failed to create the part's controls" error, which requires to restart CCS.
Please help me use EnergyTrace.
Regards,
Victor Tolosana