Hello,
I am trying to implement Packet error rate information collection. The weird thing that I have encountered is that parent event of HCI_EXT_PER, namely HCI_VE_EVENT_CODE doesn't provide connHandle information. This can be seen here in line 1071 of hci.h (this is the structure connected with HCI_VE_EVENT_CODE event):
For other events, there is often a connection handle provided - for example in line 1094.
So, my question is this really the case that we can not distinguish between connections in case of PER raport event? Or there is some other way how we can achieve it?