Other Parts Discussed in Thread: SYSCONFIG
Hello! I have a makefile project that uses SDK 5.10 that I would like to upgrade to 5.40. When building with the new SDK, drivers_cc26x21.a throws errors that GPIO_config and GPIO_pinLower/UpperBound are undefined. The 5.10 based project doesn't use GPIO.h and instead uses PIN.h and a custom GPIO implementation. I've seen the GPIO++ porting guide that claims it is a drop in replacement, but it appears I need to define those symbols somewhere to get the library working. Even though I don't use GPIO.c/h, do I *have* to port to GPIO++ to use the 5.40 driver libs?
Thanks!