Hi engineers,
My customer is reporting a wired phenomenon related to ios16. Below is the issue.
1. use an ios15 device and connect and bond to cc2642 as simple_peripheral.
2. forget the 2642 device from phone
3. update the iphone to ios16, connect to 2642
4.will restart pairing, but this pairing will fail.
5. Most wired thing here. Since problem happens in step 4, no ios device can connect to this 2642 ever again. no matter it is ios16 or lower version. Meanwhile, Android phones can still connect and bond to this 2642 as usual.
6. this issue can be saved by reset the 2642,
Any idea on this one?