Other Parts Discussed in Thread: SYSCONFIG
Hi,
Background:
rtls_responder_CC26X2R1_LAUNCHXL_tirtos7_ticlang
rtls_coordinator_CC26X2R1_LAUNCHXL_tirtos7_ticlang
SDK 6.20.00.29
Modified projects to embed MAC address inside adv data (inside GAP_DEVICE_INIT_DONE_EVENT), as such:
// AiRISTA added advertData[19] = pPkt->devAddr[0]; advertData[20] = pPkt->devAddr[1]; advertData[21] = pPkt->devAddr[2]; advertData[22] = pPkt->devAddr[3]; advertData[23] = pPkt->devAddr[4]; advertData[24] = pPkt->devAddr[5];
The problem - inside RC_EVT_ADV_REPORT event handler, when we check to make sure the MAC address reported from the stack matches the corresponding bytes inside the ADV data, we do get occasional discrepancies where BLE stack reported MAC is NOT the same as the MAC inside the adv data. We checking the last 3 of the mac because the first three bytes are never changing for our devices, and we can see the line below printing occasionally...
case RC_EVT_ADV_REPORT: { GapScan_Evt_AdvRpt_t* pAdvRpt = (GapScan_Evt_AdvRpt_t*) (pMsg->pData); uint8_t status; if (pAdvRpt->addr[2] != pAdvRpt->pData[21] || pAdvRpt->addr[1] != pAdvRpt->pData[20] || pAdvRpt->addr[0] != pAdvRpt->pData[19]) AiRISTA_DEBUG_SendDataToBackend_String("*** MISMATCH1 ***");
LOGS:
You can see the occasional "MISMATCH1" prints when MACs do not match.
At this point we have two tags advertising with primary adv interval of 100msec and periodic adv interval of 100 msec also, At this point the coordinator has synced to both tags and it is also receiving IQ samples. Our concern is if Adv Data is getting mixed up with the actual source BLE mac, is it possible this to cause the IQ samples to be mixed up between the two tags? if this is happening then obviously the angles will be wrong when calculated
Last 3 of the MACs are:
29c2 80 and 12 12 12
Lines where things are normal look like this (notice "29c280,29c280" - mac from BLE vs mac from adv data - SAME)
"2023-01-04 00:23:24:314",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,26,0,0,1,87
Lines that are mismatched (Notice "29c280,121212" - BLE MAC is 29c280 and MAC from adv data is: 121212)
2023-01-04 00:23:24:515",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-68,213,0,0,1,87
here is the code that prints these lines to help you make sense of what are we looking at:
char id_rx[12]; char id_tx[12]; char ble_tx[7]; char ble_tx_adv[7]; char interval[7]; char rssi[5]; itoa(AIRISTA_LOC_ID, id_rx,10); itoa(((pAdvRpt->addr[2]<<16) + (pAdvRpt->addr[1]<<8) + pAdvRpt->addr[0]), id_tx, 10); itoa(((pAdvRpt->addr[2]<<16) + (pAdvRpt->addr[1]<<8) + pAdvRpt->addr[0]), ble_tx, 16);//THIS IS MAC FROM BLE STACK itoa(((pAdvRpt->pData[21]<<16) + (pAdvRpt->pData[20]<<8) + pAdvRpt->pData[19]), ble_tx_adv, 16); //THIS IS MAC FROM Adv Data itoa(pAdvRpt->periodicAdvInt,interval,10); itoa(pAdvRpt->rssi,rssi,10); //2022/09/26 - change the @ to $ sign before AdvRpt //strcpy(buffer, "@AdvRpt,"); strcpy(buffer, "$AdvRpt,"); strcat(buffer,id_rx); strcat(buffer, ","); strcat(buffer, id_tx); strcat(buffer, ","); strcat(buffer, ble_tx); strcat(buffer, ","); strcat(buffer, ble_tx_adv); strcat(buffer, ","); strcat(buffer, interval); strcat(buffer, ","); strcat(buffer, rssi); strcat(buffer, ",");
Line 663923: "2023-01-04 00:22:52:647",$AdvRpt,2981883,1184274,121212,121212,80,-67,169,0,0,1,87 Line 663937: "2023-01-04 00:22:53:503",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,246,0,0,1,87 Line 663945: "2023-01-04 00:22:53:988",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,251,0,0,1,87 Line 663953: "2023-01-04 00:22:54:373",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-54,185,0,0,1,87 Line 663955: "2023-01-04 00:22:54:436",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,255,0,0,1,87 Line 663965: "2023-01-04 00:22:54:853",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,3,0,0,1,87 Line 663973: "2023-01-04 00:22:55:222",$AdvRpt,2981883,1184274,121212,121212,80,-56,190,0,0,1,87 Line 663981: "2023-01-04 00:22:55:706",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,11,0,0,1,87 Line 663983: "2023-01-04 00:22:55:738",$AdvRpt,2981883,1184274,121212,121212,80,-60,197,0,0,1,87 Line 663989: "2023-01-04 00:22:55:922",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,13,0,0,1,87 Line 663991: "2023-01-04 00:22:55:954",$AdvRpt,2981883,1184274,121212,121212,80,-60,199,0,0,1,87 Line 664005: "2023-01-04 00:22:56:776",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,18,0,0,1,87 Line 664007: "2023-01-04 00:22:56:776",$AdvRpt,2981883,1184274,121212,121212,80,-67,207,0,0,1,87 Line 664009: "2023-01-04 00:22:56:870",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,22,0,0,1,87 Line 664015: "2023-01-04 00:22:57:076",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,24,0,0,1,87 Line 664027: "2023-01-04 00:22:57:856",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-67,217,0,0,1,87 Line 664035: "2023-01-04 00:22:58:146",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,34,0,0,1,87 Line 664043: "2023-01-04 00:22:58:542",$AdvRpt,2981883,2736768,29c280,29c280,80,-48,38,0,0,1,87 Line 664045: "2023-01-04 00:22:58:579",$AdvRpt,2981883,1184274,121212,121212,80,-54,224,0,0,1,87 Line 664053: "2023-01-04 00:22:59:059",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,43,0,0,1,87 Line 664059: "2023-01-04 00:22:59:228",$AdvRpt,2981883,1184274,121212,121212,80,-60,230,0,0,1,87 Line 664067: "2023-01-04 00:22:59:682",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,49,0,0,1,87 Line 664075: "2023-01-04 00:23:00:150",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-62,239,0,0,1,87 Line 664085: "2023-01-04 00:23:00:684",$AdvRpt,2981883,1184274,121212,121212,80,-67,244,0,0,1,87 Line 664093: "2023-01-04 00:23:01:116",$AdvRpt,2981883,1184274,121212,121212,80,-69,248,0,0,1,87 Line 664095: "2023-01-04 00:23:01:163",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,63,0,0,1,87 Line 664103: "2023-01-04 00:23:01:463",$AdvRpt,2981883,1184274,121212,121212,80,-70,251,0,0,1,87 Line 664111: "2023-01-04 00:23:01:848",$AdvRpt,2981883,1184274,121212,121212,80,-55,255,0,0,1,87 Line 664119: "2023-01-04 00:23:02:302",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,74,0,0,1,87 Line 664131: "2023-01-04 00:23:03:019",$AdvRpt,2981883,1184274,121212,121212,80,-59,10,0,0,1,87 Line 664139: "2023-01-04 00:23:03:467",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-47,85,0,0,1,87 Line 664145: "2023-01-04 00:23:03:636",$AdvRpt,2981883,1184274,121212,121212,80,-59,16,0,0,1,87 Line 664147: "2023-01-04 00:23:03:667",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,87,0,0,1,87 Line 664161: "2023-01-04 00:23:04:522",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,94,0,0,1,87 Line 664167: "2023-01-04 00:23:04:722",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,96,0,0,1,87 Line 664175: "2023-01-04 00:23:05:207",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-69,30,0,0,1,87 Line 664183: "2023-01-04 00:23:05:640",$AdvRpt,2981883,1184274,121212,121212,80,-68,34,0,0,1,87 Line 664189: "2023-01-04 00:23:05:824",$AdvRpt,2981883,1184274,121212,121212,80,-55,36,0,0,1,87 Line 664191: "2023-01-04 00:23:05:893",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,107,0,0,1,87 Line 664199: "2023-01-04 00:23:06:357",$AdvRpt,2981883,1184274,121212,121212,80,-54,41,0,0,1,87 Line 664201: "2023-01-04 00:23:06:425",$AdvRpt,2981883,2736768,29c280,29c280,80,-48,112,0,0,1,87 Line 664209: "2023-01-04 00:23:06:842",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,116,0,0,1,87 Line 664217: "2023-01-04 00:23:07:111",$AdvRpt,2981883,1184274,121212,121212,80,-57,46,0,0,1,87 Line 664225: "2023-01-04 00:23:07:558",$AdvRpt,2981883,1184274,121212,121212,80,-60,49,0,0,1,87 Line 664227: "2023-01-04 00:23:07:596",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,123,0,0,1,87 Line 664229: "2023-01-04 00:23:07:627",$AdvRpt,2981883,1184274,121212,121212,80,-60,53,0,0,1,87 Line 664237: "2023-01-04 00:23:08:028",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-61,57,0,0,1,87 Line 664245: "2023-01-04 00:23:08:445",$AdvRpt,2981883,1184274,121212,121212,80,-67,61,0,0,1,87 Line 664253: "2023-01-04 00:23:08:946",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,136,0,0,1,87 Line 664259: "2023-01-04 00:23:09:178",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,138,0,0,1,87 Line 664267: "2023-01-04 00:23:09:594",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-67,72,0,0,1,87 Line 664275: "2023-01-04 00:23:10:017",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,146,0,0,1,87 Line 664287: "2023-01-04 00:23:10:650",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-49,152,0,0,1,87 Line 664295: "2023-01-04 00:23:11:152",$AdvRpt,2981883,1184274,121212,121212,80,-60,87,0,0,1,87 Line 664301: "2023-01-04 00:23:11:352",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,159,0,0,1,87 Line 664309: "2023-01-04 00:23:11:769",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,163,0,0,1,87 Line 664321: "2023-01-04 00:23:12:401",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-67,99,0,0,1,87 Line 664339: "2023-01-04 00:23:13:508",$AdvRpt,2981883,1184274,121212,121212,80,-68,108,0,0,1,87 Line 664341: "2023-01-04 00:23:13:571",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,180,0,0,1,87 Line 664349: "2023-01-04 00:23:13:925",$AdvRpt,2981883,1184274,121212,121212,80,-55,110,0,0,1,87 Line 664357: "2023-01-04 00:23:14:411",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,188,0,0,1,87 Line 664359: "2023-01-04 00:23:14:411",$AdvRpt,2981883,1184274,121212,121212,80,-55,118,0,0,1,87 Line 664365: "2023-01-04 00:23:14:628",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-57,120,0,0,1,87 Line 664367: "2023-01-04 00:23:14:628",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,190,0,0,1,87 Line 664375: "2023-01-04 00:23:15:092",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-60,124,0,0,1,87 Line 664383: "2023-01-04 00:23:15:562",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,199,0,0,1,87 Line 664389: "2023-01-04 00:23:15:762",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,201,0,0,1,87 Line 664391: "2023-01-04 00:23:15:762",$AdvRpt,2981883,1184274,121212,121212,80,-62,131,0,0,1,87 Line 664399: "2023-01-04 00:23:16:194",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,205,0,0,1,87 Line 664407: "2023-01-04 00:23:16:579",$AdvRpt,2981883,1184274,121212,121212,80,-67,135,0,0,1,87 Line 664409: "2023-01-04 00:23:16:611",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,209,0,0,1,87 Line 664411: "2023-01-04 00:23:16:633",$AdvRpt,2981883,1184274,121212,121212,80,-68,139,0,0,1,87 Line 664417: "2023-01-04 00:23:16:817",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,211,0,0,1,87 Line 664425: "2023-01-04 00:23:17:250",$AdvRpt,2981883,1184274,121212,121212,80,-68,145,0,0,1,87 Line 664433: "2023-01-04 00:23:17:751",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,220,0,0,1,87 Line 664439: "2023-01-04 00:23:17:951",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-48,222,0,0,1,87 Line 664447: "2023-01-04 00:23:18:368",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-49,226,0,0,1,87 Line 664455: "2023-01-04 00:23:18:785",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-50,230,0,0,1,87 Line 664457: "2023-01-04 00:23:18:785",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-60,160,0,0,1,87 Line 664463: "2023-01-04 00:23:19:001",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,232,0,0,1,87 Line 664465: "2023-01-04 00:23:19:001",$AdvRpt,2981883,1184274,121212,121212,80,-60,162,0,0,1,87 Line 664483: "2023-01-04 00:23:20:086",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,241,0,0,1,87 Line 664491: "2023-01-04 00:23:20:619",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,247,0,0,1,87 Line 664499: "2023-01-04 00:23:21:021",$AdvRpt,2981883,1184274,121212,121212,80,-70,181,0,0,1,87 Line 664505: "2023-01-04 00:23:21:221",$AdvRpt,2981883,1184274,121212,121212,80,-67,183,0,0,1,87 Line 664507: "2023-01-04 00:23:21:244",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,253,0,0,1,87 Line 664515: "2023-01-04 00:23:21:661",$AdvRpt,2981883,2736768,29c280,29c280,80,-50,1,0,0,1,87 Line 664523: "2023-01-04 00:23:22:093",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-50,5,0,0,1,87 Line 664531: "2023-01-04 00:23:22:579",$AdvRpt,2981883,1184274,121212,121212,80,-60,196,0,0,1,87 Line 664539: "2023-01-04 00:23:22:995",$AdvRpt,2981883,1184274,121212,121212,80,-59,200,0,0,1,87 Line 664549: "2023-01-04 00:23:23:396",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,14,0,0,1,87 Line 664551: "2023-01-04 00:23:23:396",$AdvRpt,2981883,1184274,121212,121212,80,-61,204,0,0,1,87 Line 664559: "2023-01-04 00:23:23:866",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-65,208,0,0,1,87 Line 664567: "2023-01-04 00:23:24:314",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,26,0,0,1,87 Line 664573: "2023-01-04 00:23:24:515",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-68,213,0,0,1,87 Line 664575: "2023-01-04 00:23:24:537",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,28,0,0,1,87 Line 664577: "2023-01-04 00:23:24:569",$AdvRpt,2981883,1184274,121212,121212,80,-70,215,0,0,1,87 Line 664585: "2023-01-04 00:23:24:985",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-68,219,0,0,1,87 Line 664593: "2023-01-04 00:23:25:370",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,36,0,0,1,87 Line 664595: "2023-01-04 00:23:25:417",$AdvRpt,2981883,1184274,121212,121212,80,-55,222,0,0,1,87 Line 664605: "2023-01-04 00:23:25:939",$AdvRpt,2981883,1184274,121212,121212,80,-54,227,0,0,1,87 Line 664607: "2023-01-04 00:23:26:017",$AdvRpt,2981883,2736768,29c280,29c280,80,-48,42,0,0,1,87 Line 664615: "2023-01-04 00:23:26:433",$AdvRpt,2981883,2736768,29c280,29c280,80,-49,46,0,0,1,87 Line 664617: "2023-01-04 00:23:26:433",$AdvRpt,2981883,1184274,121212,121212,80,-58,232,0,0,1,87 Line 664625: "2023-01-04 00:23:26:772",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-60,235,0,0,1,87 Line 664633: "2023-01-04 00:23:27:173",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,53,0,0,1,87 Line 664635: "2023-01-04 00:23:27:204",$AdvRpt,2981883,1184274,121212,121212,80,-60,239,0,0,1,87 Line 664647: "2023-01-04 00:23:27:807",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,59,0,0,1,87 Line 664655: "2023-01-04 00:23:28:246",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,63,0,0,1,87 Line 664667: "2023-01-04 00:23:28:910",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-70,254,0,0,1,87 Line 664675: "2023-01-04 00:23:29:380",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,74,0,0,1,87 Line 664677: "2023-01-04 00:23:29:411",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-55,4,0,0,1,87 Line 664685: "2023-01-04 00:23:29:897",$AdvRpt,2981883,2736768,29c280,29c280,80,-48,79,0,0,1,87 Line 664687: "2023-01-04 00:23:29:897",$AdvRpt,2981883,1184274,121212,121212,80,-55,9,0,0,1,87 Line 664695: "2023-01-04 00:23:30:252",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-57,12,0,0,1,87 Line 664711: "2023-01-04 00:23:31:116",$AdvRpt,2981883,1184274,121212,121212,80,-60,17,0,0,1,87 Line 664713: "2023-01-04 00:23:31:170",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-60,21,0,0,1,87 Line 664721: "2023-01-04 00:23:31:586",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,95,0,0,1,87 Line 664739: "2023-01-04 00:23:32:720",$AdvRpt,2981883,1184274,121212,121212,80,-70,36,0,0,1,87 Line 664747: "2023-01-04 00:23:33:158",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,110,0,0,1,87 Line 664753: "2023-01-04 00:23:33:352",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-54,42,0,0,1,87 Line 664755: "2023-01-04 00:23:33:390",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-47,112,0,0,1,87 Line 664763: "2023-01-04 00:23:33:807",$AdvRpt,2981883,2736768,29c280,29c280,80,-48,116,0,0,1,87 Line 664771: "2023-01-04 00:23:34:224",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-49,120,0,0,1,87 Line 664777: "2023-01-04 00:23:34:409",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-48,122,0,0,1,87 Line 664785: "2023-01-04 00:23:34:980",$AdvRpt,2981883,2736768,29c280,29c280,80,-47,127,0,0,1,87 Line 664787: "2023-01-04 00:23:35:027",$AdvRpt,2981883,1184274,121212,121212,80,-60,57,0,0,1,87 Line 664795: "2023-01-04 00:23:35:397",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,131,0,0,1,87 Line 664797: "2023-01-04 00:23:35:428",$AdvRpt,2981883,1184274,121212,121212,80,-62,61,0,0,1,87 Line 664805: "2023-01-04 00:23:35:898",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,136,0,0,1,87 Line 664813: "2023-01-04 00:23:36:268",$AdvRpt,2981883,1184274,121212,121212,80,-69,69,0,0,1,87 Line 664821: "2023-01-04 00:23:36:647",$AdvRpt,2981883,2736768,29c280,29c280,80,-45,143,0,0,1,87 Line 664829: "2023-01-04 00:23:37:064",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-46,147,0,0,1,87 Line 664831: "2023-01-04 00:23:37:117",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-55,77,0,0,1,87 Line 664839: "2023-01-04 00:23:37:470",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-47,151,0,0,1,87 Line 664845: "2023-01-04 00:23:37:687",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-48,153,0,0,1,87 Line 664847: "2023-01-04 00:23:37:771",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-55,83,0,0,1,87 Line 664861: "2023-01-04 00:23:38:636",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-47,162,0,0,1,87 Line 664867: "2023-01-04 00:23:38:836",*** MISMATCH1 ***$AdvRpt,2981883,1184274,121212,29c280,80,-47,164,0,0,1,87 Line 664875: "2023-01-04 00:23:39:236",*** MISMATCH1 ***$AdvRpt,2981883,2736768,29c280,121212,80,-61,97,0,0,1,87 Line 664877: "2023-01-04 00:23:39:236",$AdvRpt,2981883,2736768,29c280,29c280,80,-46,168,0,0,1,87 Line 664889: "2023-01-04 00:23:39:921",$AdvRpt,2981883,1184274,121212,121212,80,-67,102,0,0,1,87 Line 664891: "2023-01-04 00:23:39:975",$AdvRpt,2981883,1184274,121212,121212,80,-68,104,0,0,1,87