This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: Looking for a devices that does 802.15.4 and BLE for wireless

Part Number: CC2652R
Other Parts Discussed in Thread: CC2642R, ,

Hi Team,

Is the CC2652R the best device to select if I need 802.15.4 and BLE for wireless? Would the CC2642R be an option for that?

-Jared

  • Hi Jared,

    The CC2642R only supports BLE, so the CC2652R is a good selection for both 15.4 and BLE.  DMM can be used if the two stacks need to be operated consecutively.  You could also consider the CC2652R7 for more memory if a larger application footprint is planned, as if you need two protocols stored on the device then this will increase the base memory size requirements.

    Regards,
    Ryan