This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: PCB antenna design

Part Number: CC2642R

The PCB trace antenna is used with CC2642R. As current choice, SWRU120D is choosed as target design. But as checked in the reference design, the dxf file in document 'swrr034c' use the wrong parameters. It looks like the dxf used unit inch to replace mil by mistake. In the meanwhile, the unit in the gerber file is correct.

Could you please check if it's the true?

And give me your proposal if there is one.

Thnaks.

  • Hi Xiusheng,

    I reviewed the DXF. It looks like the intended scale for the drawing is 1000:1in so effectively the units are in mils (1/1000 of an inch). DXF are unitless without a scale being defined.

    For the gerbers, if you're using a viewer like Gerbtool or similar, you should be able to select the units you want to use.

    I looked at both files supplied, and they agree with each other with maybe the difference of 2 or 3 mil (1/000 in).

    -Jake