Other Parts Discussed in Thread: MSP430FR2433, ENERGYTRACE
Hi,team;
I used CC2640R2F launchpad to write the routine of simple_periferal and simple_broadcast. I used energytrace to check the power consumption through a MSP430FR2433.When it is not broadcast, there is about 70uA current (regardless of the broadcast interval of 1s or 5s or 10s).Confirm POWER_ SAVING has been predefined (set in project-properties). Attempted to add power directly to simple task fxn_ Sleep (0x1), which stops broadcasting, but there is still 70uA current. If the pingstandby routine is written, the power consumption will reach below 1UA.
Would you like to ask whether this is because the simple routine itself cannot enter the standby state or other reasons?
Best regards,