Dear Team,
We are working on CC2340R5 & want to connect up to 8 simultaneous connections to the board running basic_ble (*Acting as a peripheral device), but the problem we are facing is that it(*peripheral device) fails to connects more device after 2 connections (*I have used mobile phone as central devices). The Max Number of Connections set in the syscfg is 8.
Please go through the details.
SDK Version: 6.40_eng
Example: ...ti\simplelink_cc23xx_sdk_6_40_00_21_eng\examples\rtos\LP_EM_CC2340R5\ble5stack\basic_ble
UART LOG: When 3rd mobile phone tries to connect
SYSCFG
SRAM Usage
Is there anything which I am missing out or I need to change anything at the code level.
Thanks & Regards,
Harinder Singh