Other Parts Discussed in Thread: CC2640, MSP430FR2433, ENERGYTRACE,
The broadcast time of the chip is theoretically on the order of us~ms, but by observing the power consumption, the broadcast time seems to be around 1 s.
Doubt with The _pend() mechanism is relevant because if you comment out_ The pend() function,Because if you comment out _pend() function,
The broadcast is still running normally, and the high power consumption peak has been greatly shortened, but this also leads to a sharp increase in static power consumption
(This may be due to the failure of the relevant power scheduling due to the absence of a pend)
So my question is, why is the broadcast duration as long as 1 s during the pend process? Is it possible to solve it?