Other Parts Discussed in Thread: CC2340R5
Hi expert,
Hardware: CC2340R5 pg2.0 evm + host test example in 7.10.0.35 sdk + btool.
- use cc2340r5 evm to connect the other device.
-use energy trace to measure the current ~2.38mA
-set different Txpower by using btool
-OpCode : 0xFC01 (HCIExt_SetTxPowerCmd)
- the current from energy trace is the same.
it seems that txpower hci command doesn't work.
by the way, when I set HCI txPower command, there has only tx and no rx command complete event.
Is that correct?
[110] : <Tx> - 03:04:39.432
-Type : 0x01 (Command)
-OpCode : 0xFC01 (HCIExt_SetTxPowerCmd)
-Data Length : 0x01 (1) byte(s)
Tx Power : 0x09 (9) (HCI_EXT_TX_POWER_0_DBM)
Dump(Tx):
0000:01 01 FC 01 09 .....
--------------------------------------------------------------------
BR,
frank