Hi Team,
Hope you are doing good. I am reaching you in order to inquire about the availability of any component that can perform wireless data communication from an implantable device (inside a human body) to an external communicating device about 5-10 meters away (Tx-Rx gap). The protocol should be BLE and frequency should be 2.4 GHz.
Other requirements are:
1. Can support location finding or direction finding
2. Small enough to be used inside an implantable device
Currently, we have found CC2652R to be suitable for our application. This inquiry is to confirm whether CC2652R is able to fulfill our requirements. I would highly appreciate if you can comment or give suggestions because we are about to buy few components and development kits for it.
Thanks