We see the situation that the Bluetooth will disconnect or easy interrupt from the EMC Conducted Susceptibility test with CC2340R5.
The Conducted Susceptibility which belongs to EN30149.
During the test will put the nosie source from the AC adaptor when the about to 9M~10MHz frquency that the BLE signal will disconnect.
so please help if seem any situation like this or any help to fix this problem to pass the EMC test
By the way, the power for the CC2340 is stable and we did put the bead from both power or antenta from schematic.
The FW for BLE is host_test_LP_EM_CC2340R5_freertos_ticlang.out