Other Parts Discussed in Thread: UNIFLASH
Hi,
I’m working with CC2640R2F and simplelink_cc2640r2_sdk_4_20_00_04.
For my project I need to have a device with OAD off-chip capabilities, so I followed all the steps suggested in Task 2 – Add OAD to Multi Role
I successfully added OAD to the multi_role
project, and I performed successfully an OAD to update simple_peripheral_oad_offchip
to multi_role,
but then multi role FAILS to work,
as follow
***ERROR***
< Next Item
>> INTERNAL ERROR!
0xFCA89BEDD763
Connected to 1
Can't adv: no links
OAD version: 0001
Param Update 0
0x546C0EA047E5
Then if I try to perform an OAD to update multi_role to simple_peripheral_oad_offchip again, the Sending Image FAILS with Status "OAD Failure: Pairing is Required".
If I start from simple_peripheral_oad_offchip (SOFTWARE version 0001) and I perform an OAD off-chip to simple_peripheral_oad_offchip (SOFTWARE version 0002), all is OK.
Any suggestions to solve my problem?
Thanks,
Emanuela Genco