This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2642R: Issue in enabling Print logs in RTLS responder

Part Number: CC2642R
Other Parts Discussed in Thread: SYSCONFIG, CC2650

Hi,

  • Iam facing the below mentioned issues in rtls_responder code. The sdk that Iam using is simplelink_cc13x2_26x2_sdk_3_40_00_02. The CC2642R is used as the tag ,which is not advertising cte packet continuosly, there is a frequent disconnection from advertisement. It stops advertising for specific seconds but  not in a regular interval.What can be the cause of this issue?
  • Inorder to debug the issue I tried to put some print logs in the code.I have enabled uart2  in sysconfig like image_1 and image_2 below and the print logs I have written in a function like image_3. But Iam not getting any uart logs in console. How to resolve this issue ?

image_1   image_2