This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652P: zigbee传输速度较快时丢包

Part Number: CC2652P

说明:这是一个关于zigbee的问题,因论坛选择框只有“bluetooth forum”可选项,所以被划分至蓝牙论坛了。

芯片: CC2652P

协议栈版本号:simplelink_cc13xx_cc26xx_sdk_6_40_00_13

应用场景:一个协调器,一个子设备,当作透传模块使用。测试速率:每间隔30ms发送一包数据,zcl payload携带64字节数据。测试过程中,发现丢包的情况。发送端的打印LOG显示,所有数据发送成功,未出现丢包的情况,使用抓包工具抓包验证,确实是发送成功了。所以判定是接收端出现了丢包的情况。在函数void afIncomingData(...)中,增加log打印输出,通过LOG确认是丢包了。

问题:协议栈可支持最高的传输速率是多少,是否支持每间隔30ms发送64 bytes数据?

  • Good morning!

    This forum is for English communications. Could you please be so kind to post this question on the following e2e forum: e2echina.

    You could also translate your message to English and post it in this very same forum.

    Thanks!

    David.