This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2340R5: CC2340R5 PER test harmonic issue

Part Number: CC2340R5

Hi Ti,

I have two question about CC2340R5 RF performance

1. I set output power level form 0dBm to 8dBm then check power. I find there is a big difference power level at 2~5 dBm. Is this normal? Because the max delta power is -0.32dB, I would use 0.82dB as the standard.

2. I find there is an hormonic tone when I use HCI_LE_EnhancedReceiverTest command. Is this normal?

Thanks.