Part Number: CC2640R2L
Other Parts Discussed in Thread: CC2652P,
hi Expert,
Is the HCI command 'ADV_RPT_INC_CHANNEL 'Supported in the CC2640R2?
BR,
frank
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Frank,
Thank you for reaching out.
I am not familiar with the command you have mentioned and I could not find it in the Bluetooth Spec.
May I kindly ask you to point me to a place where I can get more details on this command?
Appreciate your help,
Best regards,
Hi Clément,
We follow as below to add the channel number to the host_test scan report in CC2652P.
Now, we want to do the same feature in the CC2640R2. We need to confirm if it is possible to implement.
e2e.ti.com/.../cc2652p-add-channel-number-in-host_test-scan-report
Regards,
Rote
Hi,
May I kindly ask you to specify whether you want to collect the channel number for the primary channels? If yes, one option could be to scan on only one channel.
Getting the secondary channel number won't be possible as it requires elements at the radio level.
Best regards,
Hi Clément,
We want to implement the feature as I provided the link previously.
e2e.ti.com/.../cc2652p-add-channel-number-in-host_test-scan-report
We think it can be implemented because it is working in CC2652P.
Can you help to check?
Regards,
Rote
Hi Rote,
I have checked and I am sorry, this feature is not available on the CC2640R2L device.
The CC2640R2L and CC2652P devices actually have quite some differences, this is why certain features are not available on CC2640R2L while being available on CC2652P.
Appreciate your comprehension.
Best regards,