Part Number: CC2340R5
Hello,
I am comparing power states on the CC2340R5 between the DC-DC converter and GDLO. DCDC source voltage would be 3.0V, GLDO source voltage would be 1.8V. This is the best table I can generate from the datasheet:
| CC2340R5 DCDC | Voltage | 3 | CC2340R5 GLDO | Voltage | 1.8 | |||||
| Mode | Current (uA) |
Power (uW) |
Mode | Current (uA) |
Power (uW) |
Mode | % difference CC2340R5 GLDO to DCDC | |||
| Standby LFOSC | 0.71 | 2.13 | Standby LFOSC | 1.1 | 1.98 | Standby LFOSC | -8% | |||
| Transmit 0dBm | 5100 | 15300 | Transmit 0dBM | 8800 | 15840 | Transmit 0dBM | 3% | |||
| Transmit 8dBm | 10700 | 32100 | Transmit 8dBm | 19000 | 34200 | Transmit 8dBm | 6% | |||
| Receive | 5300 | 15900 | Receive | 9000 | 16200 | Receive | 2% | |||
| UART | 24.5 | 73.5 | UART | 24.5 | 44.1 | UART | -67% | |||
| SPI | 3.4 | 10.2 | SPI | 3.4 | 6.12 | SPI | -67% | |||
| Processor Running | 2600 | 7800 | Processor Running | 4100 | 7380 | Processor Running | -6% | |||
Is it accurate to consider GLDO in this way? In the datasheet, GLDO is specified at 3.0V, but given it is an LDO, one can assume the same current draw at 1.8V.