Other Parts Discussed in Thread: UNIFLASH, , SYSCONFIG
Hi , members, I have a suggestion.
It is currently known that the ROM Bootloader of CC2340 allows the ROM to perform the Erase action by issuing a Command.
And the range of Erase cannot be changed.
Will there be a new version in the future that allows users to customize the range of Erase?
Otherwise, what should I do if there are important parameters in the Flash of CC2340 that disappear due to the update of the ROM Bootloader?
It may be possible to export important parameters through UniFlash first, but this is very troublesome. If the company's products have tens of thousands of units that need to be updated today, it is impossible for each unit to use UniFlash to export important parameters first, which will be very inefficient.
I hope this suggestion can be passed on to the development unit, thanks