Hi
I'm having trouble locating some information I need on the Bluetooth stack for use with the PAN13x5 on the Stellaris platform.
Is a piconet of 3 devices able to be set up using this platform? I found some information that indicated the piconet capabilities were limited on the MSP430 platform but have not found anything concrete about the Stellaris platform. However, the MSP430 bluetooth FAQ did mention the SPP profile demo used a piconet with multiple slaves.
Is the platform able to sink and source using the A2DP profile? I think so but would like to confirm it.
I need to target a range of 30 to 40m in a fairly open space (no obstructing walls, although there may be walls surrounding the space). It looks like the PAN13x5 can use an output power of +12dBm, which appears to be midway between Class 2 (4dBm, 10m open air) and Class 1 (20dBm, 100m open air). Is it safe to assume that the open air performance would be around 50m at maximum power output?
Cheers
Adam