Tool/software:
We measured with a BLE packet analyzer with “project_zero” written and advertised on Launchpad-cc26x2r1. Then, advertised packets and scan response packets were displayed on the analyzer.
The measurement was done with only Launchpad with project_zero written in the radio shield box.
The following is the question.
(1) Is “project_zero” designed to send scan responses when it advertises (even though there is no scan request)?
(2) If (1) is the case, is it possible to prevent it from doing so?
Best regards.