Other Parts Discussed in Thread: SYSCONFIG
Tool/software:
Hi,
We are using the CC2340R5 chipset in our development. We have are using the simpleLink_f3_sdk.
IDE: CCS
We have imported the Basic BLE project from the SDK for the CC2340R5 and have measured the active current and sleep current on the EVK using a power monitor tool.
We see that the active current during advertisement on average is about ~5.2 mA and during standby the current consumption is about 10uA.
However, in the datasheet it is mentioned that during standby mode the average current consumption is ~710nA(0.71uA).
From earlier discussion with the TI experts it was told to us that the application code does not control the wakeup/sleep sequence and this is handled by the BLE stack.
Is there something that we have to change/add to get the above desired current? As mentioned, we are currently seeing the average current consumption of 10uA when in standby mode which is a big deviation reported from the datasheet.
I have also disabled the advertising to check the device's current consumption during standby and found the average current consumption to be the same(10uA).
I have added snapshot for reference.