Hi,
I would like to develop wireless bridge chip based solution to an ANT device.
I need it to be low cost and low power consumption.
I want to use TI’s CC430 as the RF module combined with the CC2571 on the end point device.
What is the most suitable development kit?
I thought of using the EM430F6137RF900 dev kit combined with CC2571 module – would it be possible ?
Also note that I already have the ANT+ BT Health and fitness aggregator kit which contains the
• ANT UIF board - USB stick
• C7 ANT Module - based on CC2571
Aggregator
• PAN13xxETU
• MSP430 Experimenter Board
- MSP430BT5190 device
- 6 pin jumper
Bluetooth connection
• TI wireless USB stick
MSP430 USB Debugging Interface
• MSP-FET430UIF
Is it useful for my needs or should I order the EM430F6137RF900 instead ?
Thanks,
Nir