Hi,
For BLE, if I want to send data that is more than 20 bytes in a connection event. Does the programs split them up and let you send them or would I have to implement my own code? I see that others had sent multiple packets but I was not sure if they had to add their own code to the sample codes or not. If they did, was it similar to the data throughput example? Also I read that the attribute value can be up to 512 bytes but is that possible with BLE devices yet? I tried to find that explanation in the Core specs but I couldn't find it. Thank you.
Serena