I desire to use the I2C features of my CC2541EMK which is powered by a SoC_BB.
However when looking at the schematic layout of the CC2541EMK (http://pdf1.alldatasheet.com/datasheet-pdf/view/466992/TI1/CC2541EMK.html) and the schematic for the SoC_BB (http://www.ti.com/lit/ug/swru241/swru241.pdf) it appears the I2C pins SCL and SDA have been grounded on the SoC_BB, yet have pull up resistors on the EMK.
Have we made a mistake in seeing this? and if so which of the SoC_BB P10 and P11 pins are used for the SCL and SDA?
Regards,