Other Parts Discussed in Thread: CC2540
Hi
I have just downloaded a code size limited evaluation version of the iar workbench for cc2540 mini dk. And i could compile the project simpleBLEperipheral with no errors and warnings. I am using ble version 1.4 and iar workbench 8.20. Since this is a code size limited version of 4K, i wonder how i was able to compile.
the .map file has the following info
110 397 bytes of CODE memory
35 bytes of DATA memory (+ 73 absolute )
6 272 bytes of XDATA memory
194 bytes of IDATA memory
8 bits of BIT memory
4 145 bytes of CONST memory
Errors: none
Warnings: none
Can you please clarify?