This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PAN1323 3Mbps firmware?



Hi,

I'm working on second revision of a BeagleBone cape that integrates the PAN1323 module allowing the BB to stream to BT speakers. Primary usage will be for A2DP streaming..

On the first revision I used the PAN1325 and got the streaming working quite well with Bluez and TIInit_6.6.15.bts built for 3Mbps UART baud rate. All audio is transferred through the HCI interface, no I2S used.. But I started seeing consistent and periodic cutouts while streaming with the same FW and SW and the new 1323 module.

Is it that I need a different .bts file? Most likely that is the case.. But on the CC256x download page I see a FW file only for 115,2kbps baud rate.

Where can I find 3Mpbs one?

Thanks