Hi TI Folks,
Sorry, I am very new to the FCC and got a bit confused. Therefore could some experienced Engineers advise on the below question?
With regards to the FCC 15.249, there is a criteria of Electric Field of less than 50mV/m @ 3m. But from calculation, using the lowest power setting of 0dBm from the CC2564, the Electric Field is greater than 50mV/m(around 60++).
How can we pass FCC 15.249? (use attenuation circuit to reduce the output power?)
If with the lowest power setting we are facing such violation in the FCC 15.249, it is still meaningful to have high power settings?
Please find below extract from :
http://processors.wiki.ti.com/index.php/CC256x_FCC_Certification_Guide under
- White paper from bluetooth.org on LE testing: https://www.bluetooth.org/docman/handlers/downloaddoc.ashx?doc_id=237781
10.3 FCC 15.249
Another FCC study was the filing of Bluetooth LE under FCC 15.249. These rules allow for flexibility in implementing low power short-range radio systems. The rules do not restrict frequency band usage as much as in FCC 15.247. In line with FCC 15.249, the system may either be frequency hopping or stationary. The problem is that although Bluetooth LE is considered a low duty cycle system, the allowable transmission power would be too limited. The output power limits for the FCC 15.249 are:
• Maximum average transmission power -1.25 dB (radiated measurement)
• Maximum peak power +18.75 dBm (peak field strength of any emission shall not exceed the maximum permitted average limits by more than 20 dB under any condition of modulation.)
The measurement setup defined in ANSI C63.4-1992 (shown in Figure 1), decreases the calculated average radiated power from the device. The maximum allowed field intensity at a distance of 3 meters is 50 mV/m. There are two reasons why the actual output power is less than a direct conversion from the field strength to the conducted power.
• The measurement is performed to strongest polarization and direction. Non-directional applications must therefore assume an average antenna gain in their link budget calculations; therefore 2-4dBs are lost depending on antenna pattern.
• Measurement shall be performed with a reflective floor. Maximum signal can be 6 dB more than direct signal alone.
Thus, due to ground plane reflection and antenna, the average radiated power can be only ~-10 dBm
Thank you very much.
Regards,
Weiren