I am looking for some help with iOS app and firmware on both the CC2541DK and the CC2650 Sensor Tag to use the buttons for timing.
The minor complexity is that that two devices will need to be connected to an iPhone simultaneously, and the clocks synced (resonably accurately) between the two devices, so button click between the two devices can be related to each other.
The devices will need to stay connected to the iPhone for about an hour and register all the timestamps from the button presses in a DB on within the iOS app.
I have this working using the CC2540DK-MINI, but is suffers from disconnects where you then have to re-discover the keyfob.
I'm looking for someone that can provide a fixed price working solution, base on the starting point of our exisitng working solution with CC2540DK-MINI.
Please contact me ben at scammell dot com.
Thanks, in advance.
Ben